Integrated in the powerful brushless motors of the FAULHABER BX4 family, the new Integrated Motion Controller BX4 IMC impresses users with its extensive range of functions and outstanding performance. [...] flexible for local control tasks or for discrete set-point and actual values. Of course the compact 22xx…BX4 IMC can be combined with many products from the FAULHABER product range such as the compact GPT gearheads [...] emissions and the obligatory CE label. The brushless motors with the new Integrated Motion Controller BX4 IMC are available in two lengths, having first-class volume-to-performance ratio as well as highly ...
Read more," explains Compotech's Pelle Almgren. The model finally selected was FAULHABER's BX4 series brushless DC motor with 4-pole technology and high torque. The motors are equipped with incremental encoders [...] their excellent price-performance ratio. Gyrolab xPlore contains three brushless dc motors from the BX4 series , two of which have been mounted on a linear table. They move the robotic arm horizontally to [...] are positioned accurately on the CD, directly at the inlet of the respective channel. Equipped with BX4 motors , the Gyrolab xPlore also meets the speed requirements: "Generating 112 data points takes less ...
Read morecustom solution to drive the three axes. At its heart is a brushless DC-servomotor with 4-pole technology of the 2250 BX4 series . An integrated encoder with Hall sensor sends a precise position signal to the [...] were optimized by the FAULHABER experts directly in Tramelan for this special application. The 2250 BX4 servomotor is the smallest on the market capable of performing this complex task. It also satisfies [...] to its compact design, another MCDC 3002 S is used as an additional CANopen sensor node. Motor 2232 BX4 CxD was used for the horizontal axes. Here, the entire servo electronics with CANopen interface are ...
Read moreMC V3.0 family MC 5010/5005 S MC 5004 P MC 3603 S MC 3001 B/P MCS 3242/3268 BX 4 MCS 3274 BP4 as well as the new 22xx... BX4 IMC The interfaces with USB, CAN (supported interfaces: HMS-IXXAT, Peak) and ...
Read morerequired by the Light Revolution System.” The experts from EMS identified the brushless motors of the BX4 series as the optimum solution. They were able to ensure the desired precision and repeatability of [...] respond very flexibly to changes to the system.” Thanks to the compact and lightweight design of the BX4 motors , the ideal weight was also maintained. Detailed 3D models of museum objects Of course ...
Read more25, 35, 40 and 45 mm are available. This covers peak and continuous torques of 0.3 and 0.14 Nm to 4.0 and 2.6 Nm respectively. The inertias of the load may be between 2.0 and 200 kgcm². This provides [...] dimensions." In the case of the ForTorque modules, for example, the brushless DC-motors of the B and BX4 series from FAULHABER proved convincing. The motors with their two-pole and four-pole technology are [...] continuous torques of up to 168 mN in the case of the largest variant. Similar also applies to the BX4 series. "Here we use motors with 22 mm or 32 mm diameter and continuous torques of 18 and 53 mNm r ...
Read morewithout maintenance The power for these work steps is supplied by a brushless DC-servomotor of the BX4 series from FAULHABER . In addition to a high torque, the strengths of the four-pole drive include [...] collaboration The gripper experts from the Zimmer Group knew, not only from the data sheet, that the BX4 from FAULHABER would satisfy these requirements. They had previously installed motors of this series ...
Read moreHNPM. "We have been using micromotors from Schönaich for many years. For colorDoS, we opted for a BX4 series brushless DC-servomotor from FAULHABER." Installation position of the colorDoS dosing system [...] sensors In addition to the high torque of 96 mNm, the strengths of the motor with the designation 3268… BX4 CS also include the small installation space, an extremely long service life and the integrated, h ...
Read moreseries and not at all for individualised, automatic production. But this is one of the goals of Industry 4.0 and the Industrial Internet of Things (IIoT): Individual products should be designed and equipped [...] from FAULHABER play an important role here. They detect the rotation of the brushless motors of the BX4 series , which is used by the Prolynk electronic motherboard to do the odometry, calculate AGV position [...] often heavy parts at the required speed. With respect to the ratio between volume and torque, the BX4 series is a leader on the global market. This power density is a key factor in allowing us to offer ...
Read moreresponsible for handling the shoeboxes. Here, Motion Controllers , brushless DC servomotors of the BX4 series and planetary gearheads form a drive system that extends and retracts a metal tongue. The task [...] overload behaviour For the positioning of the suction gripper along a toothed rack, Magazino uses type BX4 drives from FAULHABER. With a power of 62 watts, the brushless DCservomotors deliver rated torques ...
Read moresuch as exact positioning and speed control. High-performance motor families such as the FAULHABER BX4 or BP4 and the new BXT series, complemented by the extensive range of gearheads, optical, magnetic or ...
Read moreAutonomously driving and self-contained logistics robots are a critical component of "Intralogistics 4.0". They are used both for storage as well as removal and dispatch preparation. They optimize material [...] typical picking robot comprises a lifting column and gripper. As a drive unit, it contains, e.g., BX4 series brushless DC-servomotors with integrated motion controller and planetary gearhead . When used [...] required even when the gripper is fully extended. With a diameter of only 32 mm and a length of 85.4 mm, the brushless DC-servomotors are also very compact. This makes it possible to design the gripper ...
Read moreplatform which, depending on the configuration and equipment fitted, manages with a length of 3 to 4 meters. A rigidly linked transport system forms the basis, and the other system components depend on [...] makes the real difference The engineers from STIWA heap equal praise on the brushless motor of the BX4 2250 series. In the portal handling of the compact automation, this motor drives the swivel units that ...
Read morebusiness class of the Airbus A 319 is powered by a brushless motor that weighs just 192 grams – our 3242 BX4 model . FAULHABER motors can also be found in many safety-critical applications, such as in the locking ...
Read morewith the utmost precision. Because the requirements are so high, motors from FAULHABER, such as the BX4 series with integrated Motion Controller or the portfolio of linear DC-servomotors , are used in many ...
Read moreMPG-plus 40 – also manufactured by SCHUNK. This powerful performance is delivered by a 4-pin Brushless DC-Servomotor of the BX4-series from FAULHABER. The motor has an optimised, exceptionally high-power density [...] already proven its reliability and long service life in many applications." Brushless DC-Servomotors with 4 pole Technology Customised electronics Due to space reasons, however, the control electronics had to ...
Read moreThe PWM can, however, cause a humming noise. With the brushless DC-Servomotors used here – 2232...BX4 SC for stationary and 3153...BRC for mobile incubators (both models with integrated Speed Controller) ...
Read moremechanical blockage. In combination with an integrated Motion Controller of the CxD series, the 2232…BX4 brushless servomotor satisfies these new requirements of the technicians from INCYTOИ ® – as well as ...
Read more