Career Press Supplier
Career Press Supplier
Encoder product selection perspective blue

Encoder Support

Find answers to frequently asked questions, specific information about your products and their usage or special PLC configuration files. If you need a quotation or general information about our products please contact our sales or info[at]faulhaber.com.

FAQ

Which encoder is best for which application?

This decision is usually based on the resolution and accuracy needed as well as the most suitable functional principle (optical/magnetic) and operating temperature range of the encoder types available for the desired motor series.

For which encoder types is a second shaft end available?

If a second shaft end is needed, brushless DC-Servomotors generally use analogue Hall sensors as angle sensors. If needed, encoders are installed downstream of the other add-on components, such as brakes for example.

What line lengths are possible with/without Line Driver (RS422)?
  • Without Line Driver, line lengths of up to 1-2 m are possible with incremental encoders. In individual cases, the function may depend on other parameters, such as the motor PWM and cable installation.
  • With Line Driver and twisted-pair cables, line lengths of up to several tens of meters are conceivable. What matters in this case is the differential evaluation at the end of the line or controller. In addition to this, a connection resistance at the line end may be useful for longer line lengths in order to suppress reflections.
Which encoder types are available from FAULHABER?

FAULHABER offers encoders based on the optical and magnetic functional principles.

Which encoder interfaces are available?

FAULHABER offers encoders with quadrature interface, absolute interface (BiSS-C), analogue and digital Hall signals as well as a sin/cos interface. Other interfaces are also possible on customer request.

Does FAULHABER use standardised encoder interfaces?

Yes, standardised interfaces such as quadrature interfaces acc. to RS422, absolute interfaces acc. to BiSS-C as well as digital Hall sensors are used.

What is the difference between an encoders resolution and accuracy?
  • The resolution of an incremental encoder (4* lines per revolution) is the smallest measurable angle. FAULHABER encoders have an angular resolution of up to 0.009°. 
  • The accuracy is generally a multiple of the resolution. FAULHABER encoders achieve an accuracy of up to 0.1°. The accuracy describes the maximum deviation of the actual position from the set value. For newer products such as the IER3 and IE3, this information is provided in the data sheets.
  • You can find more detailed information on the position accuracy and repeatability in the technical information about encoders.
Do FAULHABER encoders require additional protective measures against EMC?

Additional protective measures are already incorporated in some encoders, such as the IE3 and IER3. Generally speaking, the specification limits (e.g. supply voltage range) indicated in the data sheets must be heeded. In individual cases, it may be necessary to take additional measures for the customer’s application. What is critical in this respect are primarily voltage peaks on the voltage supply and signal lines, which can lead to a latch-up effect in the sensors and cause their destruction.

Application Notes

Product

Category

Document

Category

pdf

AN 130 - AES Interface Description

Category: Essentials

Choose Language English Deutsch

pdf

AN 133 - Installation of the Multiturnencoder AEMT-12/16 L combined with MC V3.0 controller family

Category: System setup

pdf

AN 136 - Block Commutation - with Digital Hall Sensors - with Absolute Encoder

Category: Essentials

pdf

AN 144 - Quadrature interface

Category: Essentials

Choose Language English Deutsch

pdf

AN 146 - Further information on IEH2 and IEH3

Category: Essentials

pdf

AN 147 - Definition of the encoder signal criteria

Category: Essentials

pdf

AN 162 - Analog Hall Sensors

Category: Essentials

pdf

AN 163 - Digital Hall Sensors

Category: Essentials

pdf

AN 192 - Handling Instructions for Incremental Encoders

Category: System setup

Webinars

Webinar programming library example

FAULHABER Drive Systems Library in SIMULINK®

EnglishFlag of GermanyGerman

In the transition to Industry 4.0, the simulation of drive systems is becoming more and more important. With a library for the MATLAB SIMULINK® environment, FAULHABER now offers the possibility to ...

Show more
Brushless Motor in robotics smart farming

Smart drive systems for smart farming

EnglishFlag of GermanyGerman

In this webinar you will see how compact, high-quality and long lifetime drive systems from FAULHABER can be used for smart farming applications.

Show more
Webinar Hall Sensors signal diagram for drive systems

Sensors for drive systems

EnglishFlag of GermanyGerman

In this webinar you will learn about sensors used in FAULHABER drive systems. After an introduction to motor operation with and without sensors, you will see how to select the right sensor and encoder ...

Show more
FAULHABER FDC drive calculator header

Unleash the power of your application with the Drive Calculator

EnglishFlag of GermanyGerman

In this webinar we will show you how to select a drive system in just a few clicks with the FAULHABER Drive Calculator. All you need to know are the key requirements of your application.

Show more
Brushless motor in robotics in the operating room

FAULHABER Drive systems for medical applications

EnglishFlag of GermanyGerman

In this webinar you can see the main drive system technologies used in many medical applications, with specific design to meet the high-level requirements in this field. From laboratory instruments to ...

Show more
Encoder product selection perspective blue

Encoder Selection - The right encoder for your drive system

EnglishFlag of GermanyGerman

This webinar will give you insights on the purpose and applications for encoders, exploring the different FAULHABER technologies.

Show more
Portfolio group product selection perspective blue

Drive System Technology Selection

EnglishFlag of GermanyGerman

In less than 45 minutes, our webinar will get you set to select the right system for your application, based on your specific requirements and desired product characteristics.

Show more
FAULHABER FDC drive calculator header

Designing drives with the FAULHABER Drive Selection Tool

EnglishFlag of GermanyGerman

Are you unfamiliar with our products but have specific requirements in terms of operating mode and load parameters, such as the speed and torque?

Show more
Two DC-Motors from the FAULHABER SXR and GXR families with an encoder, arranged on white stages against a gray-blue background.
TechNews

New highlights for complete solutions in drive technology: With the new size of the SXR motors, the powerful motor of the new GXR family, the high-precision encoder and the matching gearhead, FAULHABER presents products that are perfectly matched to one another, come from a single source and are all…

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.