On this platform we provide you with the very latest news from FAULHABER, report on the many different application areas for FAULHABER products, publish interesting technology articles, present new products, and much more besides.
Space is a hostile environment. This – in addition to the vast distances – makes manned space travel pretty difficult. Central problems include weightlessness and exposure to cosmic radiation. Anyone planning long-duration journeys through the universe needs to be aware of and fully...
A capsule full of material samples on its way back to Earth. Exposed to centrifugal forces of up to 12 G and temperatures from -270 to 5,000 degrees Celsius at its shell. The capsule has to brave it all to bring back an answer to an existential question: What is the origin of life on...
The aerospace division of Airbus has developed the first artificial assistant for astronauts named CIMON. It has been supporting the crew of the International Space Station ISS in several experiments since June. The little helper's suitability for more significant tasks in the future...
When SEIS reaches its destination at the end of November, the most sensitive seismometer that has ever been built will begin its work on Mars. Six FAULHABER stepper motors with planetary gearheads are currently on their way through space and, after the instrument has landed, will have...
2020 is the year of the next Rover mission to Mars. The main payload of the Russian Proton rocket: the ExoMars Rover, developed by the European and Russian Space Agencies (ESA & Roskosmos). The plan is for the vehicle to be equipped with nine measuring instruments. Including one that...
Endodontics or endodontology is a specialist area of dentistry. The most common procedure is the root canal treatment that a tooth receives in the case of inflamed pulp (also known as the "dental nerve"). Many of you will have experienced this procedure at first hand: The dentist...
"The value of an idea lies in its use" - as inventor Thomas Edison once accurately put it. An attitude that is also reflected in the FAULHABER slogan "Innovation in motion driving a better tomorrow". Because: drive systems from FAULHABER enable high-quality, durable and powerful...
Faster, more efficient, more sustainable – due to global competition in industry combined with booming online trade, transport structures in intralogistics are facing new challenges. The industries' answer: Automation. From storage to shipping, key work steps are being taken over by...
FAULHABER has added another extremely compact Motion Controller without housing to its product range. The new Motion Controller is ideal for integration in equipment manufacturing and medical technology applications. With 36 V and 3 A (peak current 9 A), it covers the power range up...
In this interview, Sales Managers Mireille Deckers-Strobel and Volker Sprenger report on how they manage to focus on new market requirements more quickly.
Schönaich – With the launch of the IEP3, FAULHABER expands its product line with an incremental encoder which, thanks to the latest chip technology, achieves a very high resolution and accuracy. With a diameter of just 8 mm, the IEP3 is very lightweight and compact yet still offers a...
With the all-new Linear Actuator L product family FAULHABER is offering a unique turn-key-solution for a broad range of applications. The smaller versions 06L/08L/10L are ideal for medical, lab automation, optics & photonics or space applications. The larger versions 22L/32L using the...
Here you will find external YouTube contents for the article. Click to watch.
I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.