On this platform we provide you with the very latest news from FAULHABER, report on the many different application areas for FAULHABER products, publish interesting technology articles, present new products, and much more besides.
Future trends describe the changes and developments in all areas of society, the economy or technology that triggers a new movement or direction. Futurology analyzes these and uses certain boundary conditions to allow statements to be made about the future development. Among current...
Walking without crutches – this is something that people with certain neuromuscular disorders dream of. With the exoskeleton "Autonomyo", this dream can now be made a reality. The active walking aid supports the weakened muscles and enables an intuitive sequence of movements that...
In the age of the Internet of Things (IoT) and Industry 4.0, intralogistics play a critical role. For fully automated production from batch size one, the right parts must be transported to the production stations at the right time. With an innovative, autonomous transport system,...
Ambrosia, birch, alder, hazel: About 30% of the population are to a lesser or greater degree affected by the pollen of these and other plants, trees, and bushes. The symptoms can range from relatively mild rhinitis (hay fever) through to anaphylactic shock, which may be...
The Internet of Things makes it possible to produce individualized products automatically – in batches as small as a single product. The path of the component through the assembly process thereby takes on an entirely new meaning. In the Adaptive Machine Platform Prolynk, manufacturing...
Anyone suffering from symptoms such as a cough, fever or headaches and muscle pains today tries to ascertain as quickly as possible whether they’ve been infected with corona, a cold or the flu. This is performed most easily using a swab. The sample can then be sent to a large-scale...
"The value of an idea lies in its use" - as inventor Thomas Edison once accurately put it. An attitude that is also reflected in the FAULHABER slogan "Innovation in motion driving a better tomorrow". Because: drive systems from FAULHABER enable high-quality, durable and powerful...
Faster, more efficient, more sustainable – due to global competition in industry combined with booming online trade, transport structures in intralogistics are facing new challenges. The industries' answer: Automation. From storage to shipping, key work steps are being taken over by...
FAULHABER has added another extremely compact Motion Controller without housing to its product range. The new Motion Controller is ideal for integration in equipment manufacturing and medical technology applications. With 36 V and 3 A (peak current 9 A), it covers the power range up...
In this interview, Sales Managers Mireille Deckers-Strobel and Volker Sprenger report on how they manage to focus on new market requirements more quickly.
Schönaich – With the launch of the IEP3, FAULHABER expands its product line with an incremental encoder which, thanks to the latest chip technology, achieves a very high resolution and accuracy. With a diameter of just 8 mm, the IEP3 is very lightweight and compact yet still offers a...
With the all-new Linear Actuator L product family FAULHABER is offering a unique turn-key-solution for a broad range of applications. The smaller versions 06L/08L/10L are ideal for medical, lab automation, optics & photonics or space applications. The larger versions 22L/32L using the...
Here you will find external YouTube contents for the article. Click to watch.
I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.