Manager 7: The MC V3.0 family MC 5010/5005 S MC 5004 P MC 3603 S MC 3001 B/P MCS 3242/3268 BX 4 MCS 3274 BP4 as well as the new 22xx... BX4 IMC The interfaces with USB, CAN (supported interfaces: HMS-IXXAT, ...
Read moreas exact positioning and speed control. High-performance motor families such as the FAULHABER BX4 or BP4 and the new BXT series, complemented by the extensive range of gearheads, optical, magnetic or absolute ...
Read moreAutonomously driving and self-contained logistics robots are a critical component of "Intralogistics 4.0". They are used both for storage as well as removal and dispatch preparation. They optimize material [...] typical picking robot comprises a lifting column and gripper. As a drive unit, it contains, e.g., BX4 series brushless DC-servomotors with integrated motion controller and planetary gearhead . When used [...] required even when the gripper is fully extended. With a diameter of only 32 mm and a length of 85.4 mm, the brushless DC-servomotors are also very compact. This makes it possible to design the gripper ...
Read morepotential The six drive units in each device are supplied by FAULHABER. Their core component is the 3274 BP4 brushless motor with a diameter of 32 millimeters. It offers the most power of any motor in its size ...
Read moregraphite-commutated 3257 … CR series with the 32/3R gearheads or the brushless power pack of the 2264 … BP4 series . The motor can be equipped with radial pins to secure the suspension and to absorb the forces ...
Read moreated, i.e. driverless, driving round a circuit for the first time. “We chose the FAULHABER 3274...BP4 brushless DC-Servomotor as the actuator for the steering. We installed this parallel to the steering [...] However, municHMotorsport team wants to compete with a driverless vehicle again in the coming season. 4th place for the Stuttgart team 25 students from different technical degree courses at the University [...] explaining the technical details. The driverless racing car from the Stuttgart team achieved a respectable 4th place in the competition. ...
Read morecontrol signals are converted into the appropriate movement. At its heart is a brushless motor of the BP4 series from FAULHABER, the power of which is transferred to a lead screw. Motor and lead screw rotate ...
Read morebrushless DC-motors of the 1226…B series are implemented. Where more room is available, the larger 2264…BP4 model with the MCBL3002 motion controller is used. These drives deliver the necessary torque from the ...
Read moreThe underwater robot "Belle" is the result of intensive research and development by the students of the mechanical engineering project at ETH Zurich. It was developed to overcome the complex challenge ...
Read more