more examples of how to determine motor calculations and formulas in our tutorials. What's the difference between a "servo" motor and a regular motor? The term "servo" implies that there is a feedback [...] Choose product category DC-Motors Brushless DC-Motors Motors with integrated Electronics Stepper Motors Linear DC-Servomotors Thermal and ON/OFF behaviour for stepper motors English Show more FAULHABER [...] overdrive the motor. How long do your motors and gearheads last? This varies according to each application. Factors such as operating environment, duty cycle, input power, and how the motor or gear motor is coupled ...
Read moresupport non FAULHABER motors too? Yes we do. In the end it's a matter of the feedback-system and the parameter range of the motor. FAULHABER controllers are optimized for coreless motors. Electrical time-constants [...] time-constants of these motors are as low as 50µs. But even state of the art standard servo-motors with an electrical time constant of around 1ms are supported. In the end we will have to check the parameters [...] feedback options. BLDC-servo-motors will typically have either digital or analog hall signals. Additionally they can have an incremental encoder. Alternatively FAULHABER motors using an AES absolute encoder ...
Read more