Career Press Supplier
Career Press Supplier
Glossary istock image header

Optical encoder

An optical encoder, also known as an optical rotary encoder, is characterized by a very high position accuracy and repeatability as well as a very high signal quality. Moreover, it is not sensitive to magnetic interference and offer a significantly higher resolution than magnetic encoders.

In optical rotary encoders, a code disc with a measuring element attached to the shaft of the motor is used. A distinction is made here between reflective and transmissive optical encoders.

Reflective optical encoder

With a reflective optical encoder, the light from an LED is reflected back to the code disc by a reflective surface and collected by photodetectors. Reflective optical encoders are especially compact since the LED, the photodetectors and the electronics can be mounted on the same circuit board or even on the same chip. For these reasons, FAULHABER primarily uses reflective optical encoders.

Transmissive optical encoder

A transmissive optical encoder makes use of the transmitted light process. Here, the light from the LED passes through slits in the code disc and is collected by photodetectors on the other side of the code disc.

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.