https://gpcasoc.com.ar/

Horne Technologies cc

PO Box 536

Betty's Bay, 7141

Tel.: +27 (0)76 563 2084

info@hornet.cc

www.hornetechnologies.co.za

Building of FAULHABER MINIMOTOR SA, Croglio, Switzerland
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
Building of FAULHABER Asia Pacific Pte Ltd., Singapore
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
Building of FAULHABER Polska sp. z o.o., Poznan, Poland
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
Building of FAULHABER Italia S.r.l., Lomazzo, Italy
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
Building of FAULHABER France SAS, Montigny-le-Bretonneux, France
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
Building of FAULHABER Drive System Technology (Taicang) Co., Ltd.,Taicang, China

FAULHABER Drive System Technology (Taicang) Co., Ltd.

Eastern Block, Incubator Building, No. 6 Beijing Road West

Taicang 215400, Jiangsu Province

Tel.: +86 (0) 512 5337 2626

info@faulhaber.cn

Building of FAULHABER Benelux B.V., Eindhoven, Netherlands

FAULHABER Benelux B.V.

High Tech Campus 9

5656 AE Eindhoven

Tel.: +31 (0) 40 85155-40

info@faulhaber.nl

Building of FAULHABER Austria GmbH, Wien, Austria

FAULHABER Austria GmbH

Modecenterstraße 22/C89

1030 Wien

Tel.: +43 1 7963149-0

info@faulhaber-austria.at

ERNTEC Pty. Ltd.

15 Koornang Road

Scoresby, VIC 3179

Tel.: +61 3 9756 4000

Fax: +61 3 9753 4000

sales@erntec.net

www.erntec.net

Building of Dr. Fritz Faulhaber GmbH & Co. KG, Schönaich, Germany

Headquarter

DR. FRITZ FAULHABER GMBH & CO. KG

Faulhaberstraße 1

71101 Schönaich

Tel.: +49 7031 638 0

Fax: +49 7031 638 100

info@faulhaber.de

www.faulhaber.com

We are sorry

FAULHABER is currently not represented in the selected country.

Please contact us with your request at

Info@faulhaber.com
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
Rolf Leitner

Regional Sales Manager

Tel.: +41 (0) 79 422 3348

rolf.leitner@faulhaber.ch

Rafael Steinemann

Area Sales Manager

Tel.: +41 (0) 79 932 1645

rafael.steinemann@faulhaber.ch

Bell-type armature motor

To avoid the technical disadvantages of a T-armature motor, the bell-type armature motor was developed. Its winding is self-supporting, i.e., it is not wound on a carrier.

One therefore also speaks of a self-supporting winding, air-gap winding, bell-type armature winding or a coreless design. The lack of mechanical stabilization by the carrier is compensated for by a plastic element that connects the individual windings to one another. The transfer of torque from the winding to the shaft occurs by means of a disc – the commutator plate – which is fastened on one side in the winding. Attached to this commutator plate is the commutator, which likewise has a cylindrical shape. The entire rotor, consisting of winding, commutator plate and commutator, is reminiscent of a bell. The motor is therefore also referred to as a bell-type armature motor.

Because the otherwise typical iron plates are not present, the inertia of this type of rotor is very low in comparison to conventional rotors of DC motors. This enables high dynamics. With the coreless construction, the rotor thus also operates cogging-free and very quietly. As there are no magnetic hysteresis losses, the bell-type armature motor achieves very high levels of efficiency.

One disadvantage with this type of construction is to be taken into account, however: Without the coupling to a massive metal body, less heat can be stored in the motor. This reduces the overload capacity of bell-type armature motors and must be taken into account when selecting the optimum motor for the given application.

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.

After filling out the form you will get access to our entire webinar library for a year.

* Required field

Many thanks for your interest in our product range!

You will shortly receive an email with a confirmation link. Click the link to complete the registration process. You will then be able to access the requested content.

Please contact us if you have any questions.