Consumer
Electronically controlled movements can be found almost everywhere. The huge variety of miniature motors mirrors the broad spectrum of potential applications. In the field of miniature drives in particular, FAULHABER offers a range of powerful standard products that can easily master tasks in everyday applications.
Application Highlights
A wristwatch that "sleeps" when you take it off and wakes up when you put it back on? The Type 2 from Ressence surprises in the world of mechanical timepieces with innovative functionality and revolutionary product design.
The motors don't roar and the pace is somewhat slower. Apart from that, there are many similarities between Formula 1 and the Cybathlon competition of ETH Zurich:
The driver controls a high-tech vehicle that is subject to continuous further optimisation by a team of top-class specialists. The sporting competition is also intended to promote further development of the technology – to the benefit of people with physical disabilities.
FAULHABER is on board – with high-performance motors in the wheelchair and as a sponsor of the HSR team.
Bike
It goes without saying that the bicycle is a part of locomotion culture in Germany. 97 percent of people in Germany can ride a bike. They use bicycles not only for bike tours in their free time but also on a daily basis for shopping or commuting to work. Due to rising petrol costs and the constantly congested roads at peak times, residents of large cities in particular see the bicycle as a true alternative to the automobile. FAULHABER drives are installed here in various components.
Kinetic sculpture "Project Anthozoa"
Flowing, living movement without cogging torques,a strictly linear force-current ratio, high dynamics, exact position control: thanks to these properties, the linear DC-servomotors from FAULHABER are ideal for micropositioning tasks – or for bringing a fascinating work of art to life. The kinetic sculpture "Project Anthozoa" – a collaboration between MKT AG, flying saucer GmbH and FAULHABER.
Kinetic sculpture in an active energy house
Leaves rustling in the wind, clouds floating across the sky, waves rolling up and down. Evolution developed the human eye to notice this constant change in nature. The constant movement – unpredictable in its details and “chaotic” in the most beautiful sense – is apparently good for the soul. Why else would a fireplace fire or an aquarium have such a relaxing effect? The kinetic sculptures of Bert Schoeren also follow the principle of chaotic movement.
Piano mechanics
Nowadays, concert pianists are required to render top athletic performances. Particularly when it comes to major piano concerts, pianists often explore the outer boundaries of finger strength and concert piano mechanics. Physicist and amateur pianist Dr Antoine Letessier-Selvon aims to push these limits - with the help of a linear motor from FAULHABER.
Kinetic sculpture in the showroom
In celebration of their 100th anniversary, the BMW Group commissioned the development of the "Iconic Impulses" exhibition, which looks ahead to the future: What will mobility look like in the next 100 years? What will move people? The technical implementation of the international exhibition was undertaken by MKT AG from Olching near Munich, who relied on drives from FAULHABER.
Golf trolley
A combination of exercise, relaxation and a sporting challenge - these are the things that motivate golfers when they step onto the green. The golfer’s most important companion is a lightweight and manoeuvrable golf trolley. The latest models assist their owners as E-caddies, like the TiCad Liberty, the premium golf trolley from manufacturer TiCad. The drive for these trolleys is provided by micromotors from Schönaich.
more
Chairless chair
"Oh, my legs! Aargh, my back!" Complaints like this are not uncommon when people have to spend a long day standing up. In many cases it is not possible to sit down at work because there must not be any chairs in the way. You are therefore on your feet all day, which can be quite uncomfortable. This can have a detrimental effect on concentration and performance. It can also result in physical complaints and more time taken off work, especially amongst older employees. Swiss start-up company Noonee has now developed a solution for relieving the strain on legs and backs that is both imaginative and simple – the chairless chair.
Watch Winder
The object wouldn't be out of place in a gallery or museum. There the constant and interlocking movement of the watches would be interpreted as a three-dimensional metaphor for the eternal mystery of time. In actual fact, the sight of a rotating and revolving sculpture at an art exhibition was the "big bang" for M&E. Its founders took the fascination evoked by this work of art back to the development workshop. They combined it with sophisticated technology and exquisite details to create a luxurious product in every sense. At its heart is a motor from FAULHABER which provides gentle motion for the finest watches in the world.
Further Applications
- Consumer Hand Tools
- Consumer Electronics
- Motorized Furnishings