Modelling & Prototyping
Application Highlights
Driveless Racing Cars
more
The World in Miniature
Visit the most diverse regions of the world in just a single day: explore Las Vegas, the Alps or the Norwegian fjords in only a few hours − it is possible in the Miniatur Wunderland. Located directly along the Elbe river in Hamburg's Speicherstadt (traditional warehouse district), it features the largest model railway in the world and is one of the most exciting tourist attractions in Germany. Far more than ten million visitors have marvelled at this wonderland in the meantime, which – in an area that is some 1,300 m² large – replicates in miniature sights from Scandinavia to the USA, from quayside to the mountains peaks of our world.
more
Commercial Vehicle Replicas
Spherical Vehicle
The start of a completely new development can often be a playful instinct. In the area of technology, this means that not every feasible project can be implemented in a useful manner, but it will often create basic knowledge for later applications. more
Model steam locomotive
Footballroboter
As the football stars took to the field at the European Championship in Portugal, their non-human counterparts kicked off at the Robot Football World Championship. Even without the excitement of live broadcasts during peak viewing time, the "players" and teams gave an admirable performance. The robot team with managers from the Computing Faculty of FU Berlin accomplished great things. The players' strong sprinting and running performance was accomplished with batteries and small robust DC-motors. more
Further Applications
- Solid Modelling
- Hobby
- Scaled Prototyping