Find answers to frequently asked questions, specific information about your products and their usage or special PLC configuration files. If you need a quotation or general information about our products please contact our sales or info[at]faulhaber.com.
This decision is usually based on the resolution and accuracy needed as well as the most suitable functional principle (optical/magnetic) and operating temperature range of the encoder types available for the desired motor series.
If a second shaft end is needed, brushless DC-Servomotors generally use analogue Hall sensors as angle sensors. If needed, encoders are installed downstream of the other add-on components, such as brakes for example.
FAULHABER offers encoders based on the optical and magnetic functional principles.
FAULHABER offers encoders with quadrature interface, absolute interface (BiSS-C), analogue and digital Hall signals as well as a sin/cos interface. Other interfaces are also possible on customer request.
Yes, standardised interfaces such as quadrature interfaces acc. to RS422, absolute interfaces acc. to BiSS-C as well as digital Hall sensors are used.
Additional protective measures are already incorporated in some encoders, such as the IE3 and IER3. Generally speaking, the specification limits (e.g. supply voltage range) indicated in the data sheets must be heeded. In individual cases, it may be necessary to take additional measures for the customer’s application. What is critical in this respect are primarily voltage peaks on the voltage supply and signal lines, which can lead to a latch-up effect in the sensors and cause their destruction.
Product
Category
Document
Category
AN 130 - AES Interface Description
Category: Essentials
AN 133 - Installation of the Multiturnencoder AEMT-12/16 L combined with MC V3.0 controller family
Category: System setup
AN 136 - Block Commutation - with Digital Hall Sensors - with Absolute Encoder
Category: Essentials
AN 144 - Quadrature interface
Category: Essentials
AN 192 - Handling Instructions for Incremental Encoders
Category: System setup
FAULHABER Drive Time Basics
Getting started with Drive Electronics
Motion Controller Tuning
More videos
Sitecontent