Press Suppliers
Press Suppliers

Surgical robots

Using robotic surgery, trained physicians perform complex surgical procedures with greater precision, flexibility and control than would be possible with conventional techniques. Procedures are performed either through multiple access points (multi-port access) or through a single access point (single incision port). Surgical robots range from hand-held tools, some of which integrate multiple drive systems and are designed for one specific surgical method, to fixed multi-axis robotic systems that can be used universally for a variety of medical procedures. The latter consist of robotic arms coupled with precision instruments, high-quality camera systems used directly on site inside the patient, and the computer-based robot control system. Advancements in the areas of artificial intelligence and augmented reality will continue to drive in acceptance of such surgical robots.

The variety of systems and concepts is considerable. Depending on their use and the surgical procedure to be performed, the main types of robots which can be found in operating rooms, are articulated arm robots, SCARA robots, hexapod and tripod robots, and the so-called snake-like robots. Tension wires and pulleys or toothed belts are often used to transmit motion from the drives to the robot joints and on to the end effectors. End effectors include grippers, forceps, scissors, or electrosurgical instruments. Low backlash and precise control without overshoot are paramount. This is very often ensured by mechanical preloading of the moving parts and a correspondingly optimized motion control. 

With respect to the drive technology, this means that drives with excellent control behavior must operate with high precision and reliability during operation and must also provide full torque continuously even at standstill. In addition, compactness is important so that several drives can be arranged as closely as possible to the points of application of the tension wires. Brushless drives with gearbox and encoder, optionally with motion controller, are ideally suited for this purpose.

In systems with haptic feedback, the surgeon can feel and sense variations in resistance between layers of harder and softer tissue during surgery, avoiding injury to nerves, vessels and soft tissue. To ensure that the force reflected on the surgeon's hand corresponds as directly as possible to the force on the tissue being operated on, cogging-free drives with smooth-running gears are required for 4-quadrant operation of the drive system.

Our powerful motor families – with coreless and iron-core technology - complemented by the extensive range of gearheads, encoders as well as speed and motion controllers, are ideally suited for demanding robotics applications, not only in medicine but also in many other fields.

Brushless motor in robotics in the operating room
Highest precision and reliability
Extremely long operational lifetimes
High performance in a compact design
Low Weight
High dynamic positioning
Brushless motor in robotics in the operating room
Application
Brushless DC-Motors
DC Motors
Encoders
Medical
Robotics | The next evolution in the operating room

After taking over industry, robots are now conquering the medical sciences. The advantages are obvious: absence of fatigue, maximum precision and speed, optimum ergonomics. Experts see their use as the next evolution in the treatment of patients. Already today, robot systems are used in a number of…

Related articles

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.