Press Suppliers
Press Suppliers
FAULHABER Stepper motor in Eutect compact wire feed module for soldering and welding Header

Soldering and welding are ancient techniques for joining metals that are also ideally suited to modern, automated ­fabrication processes. To achieve reproducible results, it is important to adhere to all parameters, particularly temper­a­ture and quantity of filler ­metal. Dusslingen-based company EUTECT GmbH has taken up this challenge and has ­developed an adjustable, customizable soldering and welding wire feeder. An automatic status message about the amount of weld filler used allows for optimum dosing and provides a record of operating data. EUTECT’s soldering experts have been working with the Schönaich-based microdrive specialist FAULHABER to realize a wire feed system that is both flexible and accurate. The result is a ­compact, adaptive wire feed unit that is nevertheless highly responsive to individual requirements.

Exploiting process principles

On the one hand, there is not just one solution for the majority of technical tasks; on the other, the saying “why make something complicated when simple will do” is not fortuitous. In the area of automation in particular, less can definitely mean more. The developers of the sensitive wire feed proceeded from this basic idea. As the process principle is to deliver all filler metals to the workpiece in wire form, the new module has been designed to use a wide range of filler metals. What sounds simple in terms of the basic premise, ­however, requires a great deal of know-how when it comes to the details of the automation process. Very different parameters such as wire thickness, wire stability and workpiece geometry have to be considered for the initial settings. This is why the wire feeder module incorporates various sensors that accurately identify the current wire ­position. This allows the system to deliver thin, soft soldering wire or relatively rigid steel wires for laser welding as required. The sophisticated sensor system teaches itself the joining process. However, without drives that accurately execute the control instructions, even the best data logging and evaluation system is to no effect. This is where compact microdrives come into play.

FAULHABER Stepper motor in Eutect compact wire feed module for soldering and welding

The wire is carried to the desired position via small stepper motors with a defined increment. The delivery rate results from the number of step pulses per unit time. In addition, an optical encoder signals the actual rotation to the controller. The encoder is positioned at the ­stepper motor drive wheel, where it detects slip and variations and thus measures the actual wire length being delivered.

The large number of gear ratios offered by FAULHABER compact stepper motors means that the optimum gear ratio can be selected for each process requirement. The gear and stepper motor combination, designed to customer specification and currently offering gear ratios of between 14:1 and 134:1, allowed the ­developers to work with the action-reaction ­principle for the first time. In this case, an intelligent monitoring device measures the reaction force occurring when the wire contacts the soldering point. The high-precision 22 mm stepper motors in ­combination with the encoder enable highly accurate control of the feed. The resulting wire feeding capabilities have already set new benchmarks for ­quality and reproducibility in various soldering and welding processes. The filler wire therefore functions like a virtually non-wearing mechanical sensing device directly at the site of the weld or solder. This also means that unavoidable variations in the positioning or geometry of the workpieces can be reliably identified concurrently with the joining process at that location.

FAULHABER Stepper motor in Eutect compact drive module 1
Compact drive module comprising stepper motor with plug-on encoder
FAULHABER Stepper motor in Eutect compact drive module 2
High-precision wire delivery despite compact size

The right movement for the job in hand

The application calls for a simple motor with adjustable delivery rate and ­compression force. When comparing ­various drive systems in this respect, the two-phase stepper motor emerges as the best option. With 24 steps per ­revolution and a defined step width, it is easy to ­control. At the same time, it offers the option of a defined torque of almost 40 Nm if required. The ­compressive force of the weld filler material can therefore be maintained continuously in a wide range, while delivery rates can be easily varied, at a motor speed of more than 10,000 rpm or more than 4,000 steps per second. To guarantee the necessary ­precision, a plug-on optical encoder is additionally mounted to the drive ­control wheel. The encoders are ­capable of ­generating 100 to 500 pulses per ­revolution of the wheel shaft with or without zero reference pulse, or up to 1,024 pulses in high resolution. A reduction gear used in the application further improves the resolution at the drive roller that ultimately moves the welding wire.

Products

Stepper Motors
Cost effective positioning drive without encoder
High power density
Very high acceleration
Extremely fast change of direction possible
Long-lasting
Wide operating temperature range
Full-, half- and micro-stepping operation possible
Extremely low rotor inertia
Details
Further information

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.