Career Press Supplier
Career Press Supplier
Drive System for Space Rosetta mission header

Space Exploration

Satellites, planetary landers or other scientific equipment, exploring space, sometimes take years to reach their destination, flying through vacuum and experiencing extreme temperatures. Drives that are being used in that area must therefore work guaranteed, no matter how hard the landing on a planet was or how harsh the environment is. FAULHABER drive systems, due to their reliability, minimal installation space, weight or power demands, are always a great choice for a successful mission.

From earth to mars and even beyond: FAULHABER drives are being used in a lot of space applications. Still back at earth, for example they control the fuel flow in a rocket and thus ensure a successful and also economical launch. Reaching the earth’s orbit, they hold satellites in their exact position so that measurements are always correct or ensure a safe reentry into the earth’s atmosphere. Moving objects in zero gravity is also difficult, especially inside the cramped space of a space craft or orbital stations such as the ISS. Landing on a planet like Mars poses further challenges for the drives being used for landing or for scientific experiments right after arrival. Failure is not an option. There is positively no room for a second try. If one part fails, as small as it may be, the whole mission will fail.

Reliability is a key factor as well as minimal installation space requirements, lowest possible weight or power consumption. FAULHABER drives answer these demands and at the same time provide top notch performance. The FAULHABER DC-Micromotors, Stepper Motors, brushless DC-motors, linear motors and other motor families have already been used in successful space exploration, including missions to Mars, the Sun or inside the ISS. Often accompanied by precision gearheads, encoders or customer specific wiring to fit your needs. For a successful space mission, FAULHABER is your right choice!

Drive System for Space Rosetta mission landing
High Reliability
Minimal installation space
Lowest possible weight
Power consumption
View of Jupiter surrounded by its moons against a night-blue background
Application
Aerospace & Aviation
Brushless DC-Motors
Precision Gearheads

The JUICE (Jupiter Icy Moons Explorer) probe is on a remarkable journey: It must travel around 778 million kilometers before it reaches its destination – a mission that will take eight years in total.

Related articles

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.