Staubo Elektro-Maskin a.s.

Bjørnerudveien 12C

1266 Oslo

Tel.: +47 22 75 35 00

post@staubo.no

www.staubo.no
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
info@faulhaber.be

FAULHABER Austria GmbH

Modecenterstraße 22/C89

1030 Wien

Tel.: +43 1 7963149-0

info@faulhaber-austria.at

ERNTEC Pty. Ltd.

15 Koornang Road

Scoresby, VIC 3179

Tel.: +61 (0) 3 9756 4000

sales@erntec.com.au

www.erntec.net

Headquarter

DR. FRITZ FAULHABER GMBH & CO. KG

Daimlerstr. 23
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
Rolf Leitner

Regional Sales Manager

Tel.: +41 (0) 79 422 3348

rolf.leitner@faulhaber.ch

Rafael Steinemann

Area Sales Manager

Tel.: +41 (0) 79 932 1645

rafael.steinemann@faulhaber.ch

Glossary istock image header

Optical rotary encoders

Optical rotary encoders, also known as optical encoders, are characterized by a very high position accuracy and repeatability as well as a very high signal quality. Moreover, they are not sensitive to magnetic interference and offer a significantly higher resolution than magnetic rotary encoders.

In optical rotary encoders, a code disc with a measuring element attached to the shaft of the motor is used. A distinction is made here between reflective and transmissive optical rotary encoders.

Reflective optical rotary encoders

With reflective optical rotary encoders, the light from an LED is reflected back to the code disc by a reflective surface and collected by photodetectors. Reflective optical rotary encoders are especially compact since the LED, the photodetectors and the electronics can be mounted on the same circuit board or even on the same chip. For these reasons, FAULHABER primarily uses reflective optical rotary encoders.

Transmissive optical rotary encoders

Transmissive optical rotary encoders make use of the transmitted light process. Here, the light from the LED passes through slits in the code disc and is collected by photodetectors on the other side of the code disc.

Recommended contents

Here you will find external YouTube contents for the article. Click to watch.

I consent to being shown external contents. I am aware that personal data may be shared with third-party platforms. For more information, refer to our privacy policy.

Form for requesting access protected content

Personal Data

* Required field

Many thanks for your interest in our product range!

You will shortly receive an email with a confirmation link. Click the link to complete the registration process. You will then be able to access the requested content.

Please contact us if you have any questions.