FAULHABER GROUP
FAULHABER GROUP
IMPRESSUM SITEMAP LOG IN/REGISTRATION
International » Applications by Industry » Optical » Giant telescope
Products
Applications by Industry
Custom Solutions
News
Exhibitions & Events
Jobs & Careers
Technical Library
Contact & Catalogue
FAULHABER worldwide

Advanced drive technology goes intergalactic

Stepper Motors Position Fibre
Optics In Large Telescope


Modern astronomy is struggling with the same problems as the first celestial explorers did centuries ago. The stars shine only faintly, and the further away the star, the less light hits the Earth. This issue can only be addressed by focusing the light – in other words, the telescopes keep getting larger. Today's technology is so advanced that dealing with the ever-growing scale of telescopes is relatively simple. However, giant telescopes with stationary lenses are inflexible. Hence flexible solutions are increasingly being used, specifically the mirrors are becoming thin and adjustable and the objective lens itself is designed through individual components to be movable.
Micro-drives are used to adjust the optics in order to minimise material variances, gravitational distortion or refraction fluctuations of the atmosphere. The focus is on miniature drives with backlash-free gears and long-term reliability.

 
Not every scientist can afford a giant telescope. On the other hand, anyone can develop ingenious ideas. Therefore, data from telescopes is becoming increasingly accessible to all interested scientists around the world. China has also been contributing to the "collection of knowledge" – with LAMOST (Large Sky Area Multi-Optic Fibre Spectroscopy Telescope). Technically speaking, the principle of the telescope is very well established, based on the ideas of the Schmidt telescope. In this case, the collected photons are transferred over 4,000 individual optical fibres to the spectral analysis system. For the precise setup of the fibres, the engineers have relied on the expertise of the Swiss manufacturer PRECIstep SA.

Giant telescope
The larger the optics are, the larger the amount of collectible incident light. In the case of LAMOST, the first mirror has a ­diameter of 4 m. The light is then focused on a second mirror 20 metres away and reflected from there to the analysis unit. This unit contains 4,000 individual optical fibres, which then transfer the light. The mirrors and optical fibres are designed to transmit all light within wavelengths ­between 370 and 900 nm. In other words, the telescope has sufficient sensitivity ­ranging from ultraviolet to infrared.
In order to be able to evaluate the ­incident and gathered light in a useful way, it has to be measured exactly at the location in the detector that corresponds to the actual position in the sky. Thanks to flexible optical fibres, one is no longer bound by rigid optical limitations. On the other hand, this creates the problem of exact mapping and adjustment. The ­solution was a combination of 4,000 ­single, flexible optical fibres. These can be individually adjusted by precision motors. One major problem within this area is size: the drives have to be as small as possible. After all, the laboriously collected light has to be concentrated on the smallest possible area and with high luminance in order to analyse and recognise even the smallest, weakly illuminated objects. The key to solving this problem was provided by the stepper motor specialists of the FAULHABER GROUP. Backlash-free ­precision miniature drives are a trademark of this company, which can draw on decades of expertise in the construction of micro-drive systems and even longer experience in clock-work production.

Precise and durable mighty minis
Each single fibre strand is divided into two separately adjustable axes. This requires two drives for each, totalling 8,000 individual drives. Given the high quantity and compact packing of the drives, only 10 mm "thick" including the gears, maintenance or replacement would, of course, be extremely difficult. The ­"control cable" alone consists of over 32,000 individual strands and measures about 30 cm in diameter. In addition to the required utmost precision, the ­engineers placed particular emphasis on long-lasting reliability – without the need for subsequent intervention. This is made more difficult by operational conditions that often involve no change in the adjustment for an extended period of time but may then require specific minute movements. Thanks to experience in the ­mechanical telecommunications sector with similar requirements for precision stepper motors, the FAULHABER GROUP was able to meet this challenge without any problems – by deploying standard products. Owing to the low-wear bearings used in the motor and gears, in conjunction with optimised lubricants and backlash-free planetary gears, the overall solution delivers superior precision and outstanding reliability. Today‘s mega structures are often dependent upon the reliability of miniature drives, especially in the field of optical alignment for measur­ing devices, sensors and other precision applications. Backlash-free micro-drives are the method of choice, providing the basis for reliable computerised settings of parameters. Just as in the "big world", small-footprint precision drives are the reliable link between electronics and mechanics.

More information you can find under www.faulhaber-group.com/precistep


Modern Schmidt telescope in China
provides precision measurements in
astronomy




The parallel controllable optical fibre
positioning system allows a
simultaneous adjustment of the fibres