FAULHABER GROUP
FAULHABER GROUP
IMPRESSUM SITEMAP LOG IN/REGISTRATION
International » Applications by Industry » Industrial Tools & Equipment » Cutting Plotter
Products
Applications by Industry
Custom Solutions
News
Exhibitions & Events
Jobs & Careers
Technical Library
Contact & Catalogue
FAULHABER worldwide

Customized packaging

Miniature drives for the redesign of a cutting plotter

Practically all modern products require protective packaging for shipment and handling. Paper remains the number one choice of material because, in the form of cardboard or (corrugated) cartons, it allows a multitude of customized design options. Prototype models are essential for the quick testing of design and functionality of a new design in practice. Making them by hand is too expensive and imprecise. But handy cutting plotters come to the rescue for office use. The state-of-the-art all-rounder converts CAD data directly into finished cut samples.

Cutting systems for major series are ex-pensive; stamping tools also cost a lot of money. So it’s a good idea to test a new design on prototypes before making ex-pensive investments. The specialist in cutting equipment, Lasercomb of Notzingen, has developed a new generation of multifunctional plotters for such purposes.
Reliability, precision and an attractive price are right at the top of the specifi-cation. It requires in-depth know-how of plotter technology and powerful motors for the compact drive.

To realize the demanding specifications, the manufacturer also works together with its long-term drive supplier, FAULHABER. This means proven modules can be employed as well as the rapid and expert implementation of optimum changes to the new concept.

Compact and maintenance-friendly
Initially the demand was for the develop-ment of a small, reasonably priced plotter with all the features of its big brother. But a straightforward transfer of the concept into a smaller version was not possible; the cabling costs alone would have taken it out of the price range. Hence, the decision was made to use a compact CNC controller in the top-hat module. A second innovation was to incorporate two CAN-open nodes, thus minimizing the cabling costs. One node is responsible for the inputs/outputs as a control bus and the other – cycled at a higher frequency – operates as a control bus for the drives. This ensures rapid and precise guidance of the tool in the tool head. At the same time, it was possible to reduce the number of trailing cables to the head from
17 to just one cable, including the power supply, in the first draft.
The ProDigi plotter provides maximum performance despite its extremely compact construction. Depending on the model, work surfaces of 800 x 1,300 mm to 3,100 x 1,700 mm from the tool head are traversed at speeds of up to 100 m/min (1.66 m/s) and an acceleration of 5 m/s, saving time during empty runs. In full cutting operation, it achieves up to 30 m/min, and as a drawing plotter it can even reach 50 m/min. A simple change of tools on the head is all that is required for reconfigu-ration; the electronics then adjust the cutting or drawing parameters via the sensitive controllable motors – and all this at a very low noise level making it ideal for the office. The drive power required by the plotter and the tools is provided by state-of-the-art DC motors. Some users even produce their small series on these robust ProDigi plotters!

Custom-made DC miniature drives
Once the characteristics of the plotter were specified, the designers had to select the drive components to meet these specifications. As they have done for more than 10 years, they also started work on this with FAULHABER right from the outset. The compact dimensions of the motors in the tool head were the most important aspect in this case. Here, four motors must be mounted in a limited space for controlling the Z-axis (i.e. knife stroke movement) and the C-axis (i.e. horizontal movement of the head). Each pair of motors is responsible for a tool fixture. All motors are pre-configured with connection cables and incremental encoders. The connectors are then simply attached to a so-called "switching panel" that provides the connections for the motor and the add-on modules as well as the special plug configuration for the control side. The advantage of this solution is that, in an emergency, the cus-tomer himself can replace the motor using Plug-and-Play, which means the customary resoldering of special connections required in the past is no longer necessary. A seal against the inevitable paper dust also improves the lifetime of the robust motors – without disruptive foreign bodies, the frictional pairing of brushes/collectors is subject to much less wear.
To guide the cutting knife to the precise height, a 28 W motor with 180 mNm torque at a diameter of 35 mm and length of 57 mm is installed in the head. With a lifting spindle as a self-locking gear reduction, the cutting knife can be pre-cisely positioned with zero backlash. In contrast, complete motor gear units consisting of an 80 W motor with 530 mNm and flanged metal planet gears are used for the C-axis. The high dynamics of the DC motors permit digital table height compensation (vertical tool tracking) over the entire work surface, thereby enabling a high degree of precision. This ensures a constant distance from the tool to the vacuum table and, hence, also to the material to be processed.
Nowadays miniature drives can be individually adjusted to the desired requirements – just like their big brothers.
If the drive is matched with the appli-cation requirements from the outset, many problems and compromises that may arise with standard motors can be avoided during the design. This means special characteristics in the type of con-struction, performance, electromagnetic compatibility, Plug-and-Play or sealing against specific media are also easy to implement. The user saves his own devel-opment time and is quicker on the market with his product – an advantage that is otherwise difficult to achieve.


More information you can find under www.lasercomb.de

Flexible plotter for cutting, printing and
scanning tasks



Controller and miniature drives call for
different solutions: optimally implemented,
only a single trailing cable is now required
for the controller and power supply



Compact tool head with four motors for
two-axis control. The drive is hidden under
the cover to save space