FAULHABER GROUP
FAULHABER GROUP
IMPRESSUM SITEMAP LOG IN/REGISTRATION
Home  » FAULHABER worldwide » Dr. Fritz Faulhaber
Products
Applications
News
Exhibitions & Events
Jobs & Careers
Technical Library
Contact & Catalogue
FAULHABER GROUP

Dr. Fritz Faulhaber GmbH & Co. KG




The success story of the FAULHABER brand began over 50 years ago with the development of the progressive, skew-wound, ironless rotor coil by Dr. Fritz Faulhaber. It is the cornerstone of our unique palette of high quality, high performance drive systems which are ideal for a wide variety of applications where quality, performance, and reliablity are key.
Dr. Fritz Faulhaber GmbH & Co. KG employs over 600 highly qualified staff. Our 11500 m² facility produces millions of components and systems every year. The major portion of this production consists of complete drive systems that were custom build in close cooperation between FAULHABER engineers and our customers.
The majority of our production equipment is designed and build on site. This is our guarantee that our high quality standards will be met in all phases of production.
Technologies of Tomorrow
Our state of the art research and development facilities provide us with the tools for continuous product and process improvement. This is where the drive technologies are developed, tailor made to meet the challenges of our innovative, high-tech customer base. Our product development are highly flexible and can react to new customer challenges quickly. The close contact between our research and development department and the production ensures high quality from design to finished product.
Certified Quality with every Product
Our ISO 9001 means that our product quality is guaranteed to meet the highest standards. For the user this means greater product safety. For our customers it means reducing costly incoming inspections. Companies that operate according to ISO 9001 or are in the process of attaining certification can offer a systematic approach to cooperation with the customer with the least amount of additional effort. Our added certification according to ISO 14001 emphasizes the effort that we put into protecting our environment for future generations. This is particularly demonstrated in our choice of raw materials and the attention that we give to waste control and energy consumption in production.


Product Portfolio
    Micro Drive Systems
    Coreless DC Micromotors
    Precision Gearheads
    Encoders
    Drive Electronics
    Custom Drive Systems
[more]

Location & German Sales
Dr. Fritz Faulhaber GmbH & Co. KG
Daimlerstr. 23/25
71101 Schönaich, Germany
Tel. +49 7031 638-0
Fax +49 7031 638-100
[Map this location]